| Brief Description | |
|---|---|
|
Files:
\examples\Processing\Compression\JPEG\mE5-MA-VCL\JPEG_DualBaseAreaGray.vad \examples\Processing\Compression\JPEG\SDK\ \examples\Processing\Compression\JPEG\PyPylon\ |
|
|
Platforms:
mE5-MA-VCL |
|
|
Short Description Simple examples which show the usage of the operator JPEG_Encoder. |
|
In these VisualApplets examples we show the usage of the operator JPEG_Encoder for the compression of grayscale 8 bit images for mE5-MA-VCL, mE5-MA-VCX-QP, iF-CXP12-Q and iF-CXP12-P platform for various link configurations and input bandwidths.
For usage of the applets for the platforms imaFlex Quad and imaFlex Penta, a C++ based Framegrabber SDK application as well as a Python based PyPylon script are available. Both applications demonstrate the acquisition and decompression of the JPEG stream. The source code files can be found in the directories listed above.

Prev